from __future__ import print_function
import os
import platform
import sys
# import all the stuff from mvIMPACT Acquire into the current scope
from mvIMPACT import acquire
# import all the mvIMPACT Acquire related helper function such as 'conditionalSetProperty' into the current scope
# If you want to use this module in your code feel free to do so but make sure the 'Common' folder resides in a sub-folder of your project then
from mvIMPACT.Common import exampleHelper

# For systems with NO mvDisplay library support
#import ctypes
#import Image
#import numpy

devMgr = acquire.DeviceManager()
pDev = exampleHelper.getDeviceFromUserInput(devMgr)
if pDev == None:
    exampleHelper.requestENTERFromUser()
    sys.exit(-1)
pDev.open()

print("Please enter the number of buffers to capture followed by [ENTER]: ", end='')
framesToCapture = exampleHelper.getNumberFromUser()
if framesToCapture < 1:
    print("Invalid input! Please capture at least one image")
    sys.exit(-1)

# The mvDisplay library is only available on Windows systems for now
isDisplayModuleAvailable = platform.system() == "Windows"
if isDisplayModuleAvailable:
    display = acquire.ImageDisplayWindow("A window created from Python")
else:
    print("The mvIMPACT Acquire display library is not available on this('" + platform.system() + "') system. Consider using the PIL(Python Image Library) and numpy(Numerical Python) packages instead. Have a look at the source code of this application to get an idea how.")

fi = acquire.FunctionInterface(pDev)
statistics = acquire.Statistics(pDev)

while fi.imageRequestSingle() == acquire.DMR_NO_ERROR:
    print("Buffer queued")
pPreviousRequest = None

exampleHelper.manuallyStartAcquisitionIfNeeded(pDev, fi)
for i in range(framesToCapture):
    requestNr = fi.imageRequestWaitFor(10000)
    if fi.isRequestNrValid(requestNr):
        pRequest = fi.getRequest(requestNr)
        if pRequest.isOK:
            if i%100 == 0:
                print("Info from " + pDev.serial.read() +
                         ": " + statistics.framesPerSecond.name() + ": " + statistics.framesPerSecond.readS() +
                         ", " + statistics.errorCount.name() + ": " + statistics.errorCount.readS() +
                         ", " + statistics.captureTime_s.name() + ": " + statistics.captureTime_s.readS())
            if isDisplayModuleAvailable:
                display.GetImageDisplay().SetImage(pRequest)
                display.GetImageDisplay().Update()
            # For systems with NO mvDisplay library support
            #cbuf = (ctypes.c_char * pRequest.imageSize.read()).from_address(int(pRequest.imageData.read()))
            #channelType = numpy.uint16 if pRequest.imageChannelBitDepth.read() > 8 else numpy.uint8
            #arr = numpy.fromstring(cbuf, dtype = channelType)
            #arr.shape = (pRequest.imageHeight.read(), pRequest.imageWidth.read(), pRequest.imageChannelCount.read())

            #if channelCount == 1:
            #    img = Image.fromarray(arr)
            #else:
            #    img = Image.fromarray(arr, 'RGBA' if alpha else 'RGB')
        if pPreviousRequest != None:
            pPreviousRequest.unlock()
        pPreviousRequest = pRequest
        fi.imageRequestSingle()
    else:
        # Please note that slow systems or interface technologies in combination with high resolution sensors
        # might need more time to transmit an image than the timeout value which has been passed to imageRequestWaitFor().
        # If this is the case simply wait multiple times OR increase the timeout(not recommended as usually not necessary
        # and potentially makes the capture thread less responsive) and rebuild this application.
        # Once the device is configured for triggered image acquisition and the timeout elapsed before
        # the device has been triggered this might happen as well.
        # The return code would be -2119(DEV_WAIT_FOR_REQUEST_FAILED) in that case, the documentation will provide
        # additional information under TDMR_ERROR in the interface reference.
        # If waiting with an infinite timeout(-1) it will be necessary to call 'imageRequestReset' from another thread
        # to force 'imageRequestWaitFor' to return when no data is coming from the device/can be captured.
        print("imageRequestWaitFor failed (" + str(requestNr) + ", " + acquire.ImpactAcquireException.getErrorCodeAsString(requestNr) + ")")
exampleHelper.manuallyStopAcquisitionIfNeeded(pDev, fi)
exampleHelper.requestENTERFromUser()