<?xml version="1.0" encoding="ISO-8859-1" standalone="yes"?>
<PropList contentDescriptor="CameraLinkCameraDescription" name="CameraLink_SiliconImaging_SI-1920HD" default="0" parent="none" versionMajor="1" versionMinor="10" versionRelease="88">
  <DocString value="This camera will always work with 12 bit internally but if you want to capture only the 8 or 10 MSB of the signal the BitsPerPixel parameter can be changed. The capture device(frame grabber) will skip the other bits then."></DocString>
  <Property name="Name" default="0" >
    <Value index="0" val="SiliconImaging_SI-1920HD"></Value>
  </Property>
  <Property name="VideoOutput" default="0" >
    <Value index="0" val="Base"></Value>
  </Property>
  <PropList name="ActiveVideoAoi" default="0" parent="none">
    <Property name="X" default="0" >
      <Value index="0" val="0"></Value>
    </Property>
    <Property name="Y" default="0" >
      <Value index="0" val="0"></Value>
    </Property>
    <Property name="W" default="0" >
      <Value index="0" val="1920"></Value>
    </Property>
    <Property name="H" default="0" >
      <Value index="0" val="1080"></Value>
    </Property>
  </PropList>
  <Property name="BitsPerPixel" default="1" >
    <Value index="0" val="12"></Value>
  </Property>
  <Property name="PixelsPerCycle" default="1" >
    <Value index="0" val="2"></Value>
  </Property>
  <Property name="DataValid" default="0" >
    <Value index="0" val="InActive"></Value>
  </Property>
  <Property name="Format" default="0" >
    <Value index="0" val="Mono"></Value>
  </Property>
  <Property name="ScanMode" default="0" >
    <Value index="0" val="Area"></Value>
  </Property>
  <Property name="TapsXGeometry" default="1" >
    <Value index="0" val="1X2"></Value>
  </Property>
  <Property name="TapsYGeometry" default="1" >
    <Value index="0" val="1Y"></Value>
  </Property>
</PropList>