Linux kernel sources for mvBlueLYNX-2xx/4xx/5xx/6xx This kernel s version 2.4.25 based on development kernel at http://www.denx.de. We provide the sources as required by the GPL but do not offer any support for kernels you have compiled or changed yourself. You will need.. 1. Linux PC. 2. The 603e cross compiler for PowerPC (see latest MATRIX VISION CD). 3. Some tools from U-Boot needed to make a U-Boot image. 4. Some knowledge of building Linux kernels. For mvbl_2xx/4xx/6xx: 1. Unpack source. cd into the directory. 2. For mvbl_2xx/4xx/6xx: make mvblue_config -or- For mvbl_5xx: make mvbl_m_config 4. make oldconfig 5. make dep 6. make uImage modules July 2005