Release: 2.61.131.0
Date: 2025-02-11
|
(BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0081UG.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*) |
| Type |
Description |
(BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0081UG.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*) |
| Feature |
Added Encoder support for all BVS CA-GT cameras. |
(BVS CA-GT1-.*) |
| Feature |
The features 'mvMultiAreaMode' and 'ReverseX/Y' can now used simultaneously. |
(BVS CA-GT1-.*) |
| Feature |
The 'mvMultiZone' function, which enables different exposure and gain in one image is now available for cameras with SONY IMX Gen.4 sensors. |
(BVS CA-GT1-.*) |
| Bugfix |
Possible PTP1588 synchronizing error when the master clock device changes. |
(BVS CA-GT1-.*) |
| Bugfix |
Possible oscillation in image brightness when using AEC in conjunction with FPGA binning. |
(BVS CA-GT1-.*) |
| Feature |
The ReadOnly Properties mvTimescale and mvCurrentUtcOffset inform the user, which time base is used and, if it is TAI, which offset it has to UTC. |
(BVS CA-GT1-.*) |
| Feature |
mvPtpClockMode specifies whether the device participates in the negotiation which device becomes master (default) or is forced to be slave. |
(BVS CA-GT1-.*) |
| Improvement |
Using Exact Exposure Time for Gen4 Sensors. |
(BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0081UG.*|BVS CA-GT1-0051B.*) |
| Behaviour |
In MultiExposureMode the ExposureActive signal is now generated by the sensor. |
(BVS CA-GT1-.*) |
| Improvement |
Camera tries to restart itself after an under voltage event. |
(BVS CA-GT1-.*) |
| Feature |
Added support for GigEVision 2.2 standard for all BVS CA-GT cameras. |
(BVS CA-GT1-.*) |
| Behaviour |
Standard value of Bootstrap Register Discovery ACK Delay changed from 900ms to 100ms. |
(BVS CA-GT1-.*) |
Release: 2.55.3663.0
Date: 2023-10-10
|
(BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0081UG.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0081UG.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*) |
| Type |
Description |
(BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0081UG.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0081UG.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*) |
| Other |
MATRIX VISION mvBlueCOUGAR-XT is now Balluff BVS CA-GT. |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed bug that prevented GEV Discovery ACKs from being sent after the camera switched from LLA address to DHCP address. |
(BVS CA-GT1-.*) |
| Bugfix |
TimestampReset command did not set the timestamp to 0 if the camera was in PTP slave mode before. |
(BVS CA-GT1-.*) |
| Feature |
Implemented mvCyclicSignal that can be used together with IEEE1588 (PTP) to synchronize image acquisition between cameras without additional cabling. |
(BVS CA-GT1-.*) |
| Feature |
Implemented Short Intervall Trigger for Sony IMXv4 sensors. |
(BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0081UG.*|BVS CA-GT1-0051B.*) |
| Bugfix |
Reduced the maximum temperatures allowed before the camera switches to over temperature mode. This is to avoid problems due to overheating memory chips. |
(BVS CA-GT1-.*) |
| Bugfix |
Pixel jitter could occur with mvGammaEnable = true. |
(BVS CA-GT1-.*) |
| Feature |
Action Command with Acknowledge support. |
(BVS CA-GT1-.*) |
| Feature |
New features TestPendingAck and TestEventGenerate in category TestControl for GigEVision V2.2. |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed a bug in IMXv4 sensor control library that sometimes resulted missing images depending on AOI height. |
(BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0081UG.*|BVS CA-GT1-0051B.*) |
| Improvement |
Improved the SLVS-EC synchronization. Failed synchronization sometimes led to missing images. |
(BVS CA-GT1-.*) |
| Bugfix |
BVS CA-GT cameras no longer set the static LAG capability bit in the Physical Link Configuration Capability Register. |
(BVS CA-GT1-.*) |
Release: 2.49.3198.0
Date: 2022-08-24
|
(BVS CA-GT1-0081UG.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*) |
| Type |
Description |
(BVS CA-GT1-0081UG.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*) |
| Feature |
Initial firmware release for BVS CA-GT cameras using sensors of type Sony IMX487. |
(BVS CA-GT1-0081UG.*) |
| Behaviour |
The minimum width is now 624 (instead of 1216). |
(BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*) |
| Improvement |
Optimized IEEE1588 PTPv2 Clock-Synchronization Algorithm for better Clock-Accuracy. |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed a bug that could lead to missing frames when using Binning/Decimation with Color-Sensors. |
(BVS CA-GT1-.*) |
| Improvement |
All 64 bits of the I/O timestamps are now read from the hardware. |
(BVS CA-GT1-.*) |
| Bugfix |
Implemented the conversion of 80 bit IEEE1588 timestamps from/to 63 bit GeniCam timestamps according to the GigEVision specification. |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed a bug in the synchronization code of the internal clocks that led to timestamp errors in PTP master mode. |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed bug that caused the frame buffer to fill up very slowly when streaming with maximum speed. |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed wrong sensor register values when switching to/from binning/decimation mode. |
(BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*) |
| Bugfix |
Fixed bug that affects max. Framerate for Mono12p and Bayer12p Pixel-Formats. |
(BVS CA-GT1-.*) |
| Feature |
Added property mvDeviceFanEnable that allows the user to switch the fan on and off. |
(BVS CA-GT1-.*) |
| Improvement |
Upgraded version of filesystem. |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed bug that in GEV packet size negotiation that could have lead to invalid packet sizes. |
(BVS CA-GT1-.*) |
| Feature |
Added support for Action Commands. |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed bug that sometimes lead to missing frames after changing the image width/height. |
(BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*) |
| Bugfix |
Fixed problems in digital I/O handling which could result in missing I/O events. |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed bug that could lead to wrong over temperature events when using the camera in cold conditions. |
(BVS CA-GT1-.*) |
| Feature |
Added support for Defective Pixel Correction. |
(BVS CA-GT1-.*) |
Release: 2.45.2900.0
Date: 2021-11-15
|
(BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*) |
| Type |
Description |
(BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*|BVS CA-GT1-.*|BVS CA-GT1-.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*) |
| Bugfix |
Fixed bug that led to unintentional pulses on IO lines during camera startup when working with UserSetDefault != Default. |
(BVS CA-GT1-.*) |
| Bugfix |
DeviceLinkHeartbeatTimeoutRegister can be read back after change now. |
(BVS CA-GT1-.*) |
| Feature |
The automatic white balance (AWB) has been improved concerning the behavior when all pixels are saturated. In this case nearly no color casts arise. |
(BVS CA-GT1-.*) |
| Bugfix |
Prevented overtriggering of the sensor due to inaccurracy in framerate calculation. |
(BVS CA-GT1-.*) |
| Bugfix |
Changing exposure time could stop auto exposure control. |
(BVS CA-GT1-.*) |
| Bugfix |
Maximum Framerate has not been adjusted when AEC was activated. |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed bug when setting sensor registers (some registers were not set) |
(BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*) |
| Bugfix |
Persitent IP is now checked for IP clashed before using it. |
(BVS CA-GT1-.*) |
| Bugfix |
The value of the GVSP packet size register is now rounded down to nearest valid value if an unsupported value has been written |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed bug that prevented DHCP from being switched off completely |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed bug in GenICam XML file |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed bug that prevented device discovery using directed broadcasts after changing the subnet using FORCE_IP |
(BVS CA-GT1-.*) |
| Bugfix |
Corrected bug in frame rate calculation that occurred when binning/decimation was used and bit depth was changed afterwards |
(BVS CA-GT1-.*) |
| Feature |
Added binning/decimation support in FPGA |
(BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*|BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*) |
| Bugfix |
Fixed bug that could lead to unstable framerates when using sensor binning/decimation |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed bug that could lead to overtemperature state in case of negative temperatures |
(BVS CA-GT1-.*) |
| Bugfix |
Fixed bug that prevented acquisition of very small and fast images with IMX531 |
(BVS CA-GT1-0204Z.*) |
| Feature |
Initial firmware release for BVS CA-GT cameras using sensors of type Sony IMX535, IMX536 or IMX537 |
(BVS CA-GT1-0124B.*|BVS CA-GT1-0081Z.*|BVS CA-GT1-0051B.*) |
Release: 2.42.2708.0
Date: 2021-06-07
|
(BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*) |
| Type |
Description |
(BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*) |
| Feature |
Initial firmware release for BVS CA-GT cameras using sensors of type Sony IMX530, IMX531 or IMX532 |
(BVS CA-GT1-0246Z.*|BVS CA-GT1-0204Z.*|BVS CA-GT1-0162Z.*) |